Release Note GSAY-A4-F0-Z4-2.3.0

Firmware: 3.8.14

Note:
- Only working with CMMT/EMMT, no support of CMMP/EMMS
- A FW update from version 3.4.6 or smaller to 3.8.14 is required and it cannot be downgraded from version 3.8.14 to 3.4.6 or smaller
- A GSDML update in the higher-level plc to the version GSDML-V2.34-Festo-CECC_X-20210401.xml is required
- An update of the host function blocks is required (New host interface)

Bugs Fixes:
* BUGEA-6184576  Wrong motor configuration comparing to FAS
* BUGEA-6383054  Save button at the last programming step does not work
* BUGEA-6415725  Load Hardware Configuration failed
* BUGEA-6635973  System stays very long approx. 20s while starting up. INIT_STATE_GET_NUM_LOG_SD_CARD
* BUGEA-6854616  TCP/IP Connection frozen
* BUGEA-6863878  No Maximum force and Position when selecting without Record
* BUGEA-6900861  Wrong judgement with envelope (false OK)
* BUGEA-6958990  Press sequencer does not start, but giving part OK
* BUGEA-7034002  Wrong reaction to YJKP STO trigger
* BUGEA-7065772  Force Control does not work right after Force Mode
* BUGEA-7083845  System stays "in operation" forever
* BUGEA-7095289  PtP Error 1100 in Force Mode after run continuously within 1 hour.
* BUGEA-7115735  YJKP_BUG_FOR No max position and max force
* BUGEA-7143408  Position Mode small force limit triggers error
* BUGEA-7179652  Profinet connection disrupted
* BUGEA-7243674  Wrong test result display The name, the max values
* BUGEA-7484908  Wrong Message for Inoperation timeout - FTP,SMB,Evaluation,Statistic
* BUGEA-7771738  YJKP can't load hardware configuration to CMMT Firmware 36 (0x2288 not existing)
* BUGEA-7804824  Fake pressing result after execution
* BUGEA-8081815  Adjust force sensor - Wrong text in description
* BUGEA-8082002  Logging Configuration - Enable USB does not change label when enabled
* BUGEA-8117480  Version check for CMMT Firmware failed
* BUGEA-8118457  Language settings will not be kept after restart
* BUGEA-8127027  JobStatus not displayed as clear text
* BUGEA-8148276  Error in step mode - gsay stays in status "in operation"
* BUGEA-8158126  Press stucks at Positioning Mode after Smart Force Control
* BUGEA-8161557  "Advance force mode" with "Configure failure reaction" is not Working as Expected.
* BUGEA-8165930  Step mode - leaving step mode or reset system after pressing "abort" is not possible
* BUGEA-8168754  Record curve - 5 records enabled, only 4 displayed
* BUGEA-8168816  Record curve - recording reference curve in programming mode leads to NOK pressing in diagnosis view
* BUGEA-8169757  Bug for error reaction in force control mode
* BUGEA-8174023  Bug for Smart force control - Configure Failure reaction.
* BUGEA-8183989  Bug for Postion mode - Configure Failure reaction.
* BUGEA-8261614  Logging configuration - cancel-button does not work correctly or does not affect the display of the current status
* BUGEA-8262592  OPC UA variable cannot be seen

New Features:
* Firmware Check
* Singularity Detection


Release Note GSAY-A4-F0-Z4-2.2.0

Firmware: 3.8.14

Note:
- Only working with CMMT/EMMT, no support of CMMP/EMMS
- A FW update from version 3.4.6 or smaller to 3.8.14 is required and it cannot be downgraded from version 3.8.14 to 3.4.6 or smaller
- A GSDML update in the higher-level plc to the version GSDML-V2.34-Festo-CECC_X-20210401.xml is required
- An update of the host function blocks is required (New host interface)

Bugs Fixes:
* BUGEA-6020930 - Old data is not reset after starting a new pressing.
* BUGEA-6058778 - System freezes when xEnableSystem and xAbort are set to false simultaneously.
* BUGEA-6085252 - "Stop" button does not work for relative motion tasks in WebVisu.
* BUGEA-6123040 - False NOK status for Threshold and Window (Flex).
* BUGEA-6128118 - System reset by host PLC causes continuous switching off and on.
* BUGEA-6153389 - Inability to regulate force back to target during holding.
* BUGEA-6163574 - Relative movement fails when the target force is set lower than the actual force; no failure reaction.
* BUGEA-6166059 - System remains stuck in Advanced Force Mode.
* BUGEA-6169891 - System remains in absolute position mode indefinitely.
* BUGEA-6170916 - System remains stuck in jump mode.
* BUGEA-6171555 - System remains in relative position mode indefinitely.
* BUGEA-6178423 - System remains in force control mode.
* BUGEA-6178869 - System stays in Position Mode (In operation) - SEQUENCER_ERROR_REACTION
* BUGEA-6181969 - Force mode relative movement (distance) with variable does not work
* BUGEA-6186419 - System stays in Position Mode (In operation)
* BUGEA-6233713 - Incorrect serial number in ParameterChannel
* BUGEA-6284900 - System configuration could not be saved.
* BUGEA-6293241 - ModbusTCP is not working
* BUGEA-6363663 - No error triggered when the maximum position is reached in force mode.
* BUGEA-6363945 - AcknowledgementParameterChannel from YJKP to host always has the same value of StatusParameterChannel
* BUGEA-6383199 - Save Program doesn't work
* BUGEA-6572226 - Sample Interval of Curve is Not Constant
* BUGEA-6594116 - Programs cant be selected until button of edit been clicked.
* BUGEA-6594118 - Target force not reached,but the max position been touch,YJKP give us OK.
* BUGEA-6620239 - Wrong parameter of "target reached", monitoring window of  P1.469.0.0
* BUGEA-6635970 - First press will always be NOK
* BUGEA-6642493 - Smart Force Control not Functional
* BUGEA-6653738 - Position seems only to be updated every 20ms
* BUGEA-6670717 - Same force value sampled under Advanced Force Mode with YJKPflex Configuration
* BUGEA-6703395 - Duplicated data exist with AFM in GSAY 2.1.13RC15
* BUGEA-6724455 - Curve of force mode are not correct illustrated in version > 2.1.13 RC13

Improvement & Enhancements
* TASK-6182926 - Reverted workaround for fbStop.Done, returning to FDC 3.5.15_39.
* TASK-6185266 - Add debug logs for movement signals
* TASK-6262201 - Bring back the version indicating on webpage
* TASK-6581678 - New force control: Smart Force Control
* TASK-6660003 - Reduce cycle time from 2ms -> 1ms in Advanced Force Mode
* TASK-6789317 - Add bars for indicating actual force, actual position and actual velocity

New Features
* US-6148882 - Debuglog
* US-6233963 - Option to deactivate the Error: Read analog force value - Negative limit value reached
* US-6234222 - Indicating the system is saving logs
* US-6394460 - Increase the time limit in Advanced force mode to 2 min
* US-6642495 - Add Option for Data Aggregation in Position and Force Modes
* US-6767317 - Indicating axis is moving
* US-6767327 - Indicating error reaction


Release Note GSAY-A4-F0-Z4-2.1.12

Firmware: 3.8.14

Note:
- Only working with CMMT/EMMT, no support of CMMP/EMMS
- A FW update from version 3.4.6 or smaller to 3.8.14 is required and it cannot be downgraded from version 3.8.14 to 3.4.6 or smaller
- A GSDML update in the higher-level plc to the version GSDML-V2.34-Festo-CECC_X-20210401.xml is required
- An update of the host function blocks is required (New host interface)

Change Requests:
* TASK-6178291 - Log Implicit timelimit in Advanced Force Mode

Bugs:
* BUGEA-6020917 - Wrong description on Webvisu and error description in Chinese
* BUGEA-6044044 - "Access Violation" issue
* BUGEA-6098961 - System stuck with Force Control Kp=0
* BUGEA-6105804 - YJKP OPC UA Accessibility
* BUGEA-6105912 - Wrong translating in Spanish and German
* BUGEA-6125951 - Wrong window evaluation (Flex)
* BUGEA-6160651 - Inability to Regulate Force Back to Target During Holding (flex)
* BUGEA-6178339 - Access Violation during advanced force mode


Release Note GSAY-A4-F0-Z4-2.1.11

Firmware: 3.8.14

Note:
- Only working with CMMT/EMMT, no support of CMMP/EMMS
- A FW update from version 3.4.6 or smaller to 3.8.14 is required and it cannot be downgraded from version 3.8.14 to 3.4.6 or smaller
- A GSDML update in the higher-level plc to the version GSDML-V2.34-Festo-CECC_X-20210401.xml is required
- An update of the host function blocks is required (New host interface)

Change Requests:
* US-5404893 - More than 20 press programs (Up to 99 programs)
* US-5889145 - Logging of NOK curves only
* US-5889203 - Max force diagnosis = Max force in operations
* US-5809682 - Increase the holding time for "force control" up to 12 hours (Flex)
* US-5703174 - Indicate Host PLC When YJKP is under Webvisu Control
* US-5889164 - Additional record time after positioning (Flex)

Bugs:
* BUGEA-5248523 - No step number with NOK result


Release Note GSAY-A4-F0-Z4-2.1.9

Firmware: 3.8.14

Note:
- Only working with CMMT/EMMT, no support of CMMP/EMMS
- A FW update from version 3.4.6 or smaller to 3.8.14 is required and it cannot be downgraded from version 3.8.14 to 3.4.6 or smaller
- A GSDML update in the higher-level plc to the version GSDML-V2.34-Festo-CECC_X-20210401.xml is required
- An update of the host function blocks is required (New host interface)

Change Requests:
* US-5837930 - Indicate version number

Bugs:
* BUGEA-5680591 - Low voltage error in CMMT for 12kN (Load voltage AC 110V)
* BUGEA-5798518 - Functional failure of the Force Control Mode (12 and 17kN)
* BUGEA-5891447 - The "Log in" button seems to have changed the size of the text field (too small)
* BUGEA-5896442 - Homing didn't work
* BUGEA-5897140 - Empty error message for homing without enable


Release Note GSAY-A4-F0-Z4-2.1.7

Firmware: 3.8.14

Note:
- Only working with CMMT/EMMT, no support of CMMP/EMMS
- A FW update from version 3.4.6 or smaller to 3.8.14 is required and it cannot be downgraded from version 3.8.14 to 3.4.6 or smaller
- A GSDML update in the higher-level plc to the version GSDML-V2.34-Festo-CECC_X-20210401.xml is required
- An update of the host function blocks is required (New host interface)

Bugs:
* BUGEA-5547524 - Evaluation methods -> Sporadic false OK/NOK (Window down/up side, Force threshold) / Bewertungsverfahren -> Sporadisch Falsch OK/NOK (Fenster untere/obere Siete, Kraft-Schwellwert)


Release Note GSAY-A4-F0-Z4-2.1.5

Firmware: 3.8.14

Note:
- Only working with CMMT/EMMT, no support of CMMP/EMMS
- A FW update from version 3.4.6 or smaller to 3.8.14 is required and it cannot be downgraded from version 3.8.14 to 3.4.6 or smaller
- A GSDML update in the higher-level plc to the version GSDML-V2.34-Festo-CECC_X-20210401.xml is required
- An update of the host function blocks is required (New host interface)

Bugs:
* BUGEA-5659403 - Loss of homing-signal for multi-turn encoder after system reboot / Verlust des Homing-Signals fr Multiturn-Encoder nach Systemneustart


Release Note GSAY-A4-F0-Z4-2.1.3

Firmware: 3.8.14

Note:
- Only working with CMMT/EMMT, no support of CMMP/EMMS
- A FW update from version 3.4.6 or smaller to 3.8.14 is required and it cannot be downgraded from version 3.8.14 to 3.4.6 or smaller
- A GSDML update in the higher-level plc to the version GSDML-V2.34-Festo-CECC_X-20210401.xml is required
- An update of the host function blocks is required (New host interface)

Change Requests:
* EPIC-5379998 - YJKPflex function with CMMT-AS / YJKPflex Funktion mit CMMT-AS
	* US-5397945 - Flexible configuration of actuator / Flexible Konfiguration des Aktuators
	* US-5397946 - Flexible dynamic limits / Flexible dynamische Grenzen
* EPIC-5379527 - New evaluation tools / Neue Bewertungsverfahren	
	* US-5397908 - New evaluation tools - Force treshold type 1/2/3/4 / Neue Bewertungsverfahren - Kraft-Schwellwert Typ 1/2/3/4
* EPIC-5232392 - Release holding brake from Visu/Host / Lsen der Haltebremse von Visu/Host	
	* US-5380166 - Control holding brake by GUI / Steuern der Haltebremse ber die GUI
	* US-5380167 - Control holding brake by Host / Steuern der Haltebremse ber Host
* US-5380441 - Visual differenciation of the licenses / Optische Unterscheidung der Lizenzen
	
Bugs:
* BUGEA-5372046 - CDPX scaling issue / CDPX Skalierungsproblem
* BUGEA-5446667 - CMMT FW V32.0.9.9 Following error acceleration / CMMT FW V32.0.9.9 Schleppfehler Beschleunigung
* BUGEA-5447768 - Position and velocity in GSAY differ from FAS / Position und Geschwindigkeit in GSAY unterscheiden sich von FAS


Release Note GSAY-A4-F0-Z4-2.1.1

Firmware: 3.8.14

Note:
- Only working with CMMT/EMMT, no support of CMMP/EMMS
- A FW update from version 3.4.6 or smaller to 3.8.14 is required and it cannot be downgraded from version 3.8.14 to 3.4.6 or smaller
- A GSDML update in the higher-level plc to the version GSDML-V2.34-Festo-CECC_X-20210401.xml is required
- An update of the host function blocks is required (New host interface)

Change Requests:
* CRQ-4435172 - Migration to CMMT/EMMT / Migration auf CMMT/EMMT


Release Note GSAY-A4-F0-Z4-1.4.5

Firmware: 3.8.14

Note:
- A FW update from version 3.4.6 or smaller to 3.8.14 is required and it cannot be downgraded from version 3.8.14 to 3.4.6 or smaller
- A GSDML update in the higher-level plc to the version GSDML-V2.34-Festo-CECC_X-20210401.xml is required
- An update of the host function blocks is required (New host interface)

Bugs:
* BUGEA-5547524 - Evaluation methods -> Sporadic false OK/NOK (Window down/up side, Force threshold) / Bewertungsverfahren -> Sporadisch Falsch OK/NOK (Fenster untere/obere Siete, Kraft-Schwellwert)


Release Note GSAY-A4-F0-Z4-1.4.3

Firmware: 3.8.14

Note:
- A FW update from version 3.4.6 or smaller to 3.8.14 is required and it cannot be downgraded from version 3.8.14 to 3.4.6 or smaller
- A GSDML update in the higher-level plc to the version GSDML-V2.34-Festo-CECC_X-20210401.xml is required
- An update of the host function blocks is required (New host interface)

Change Requests:
* CRQ-5987896 - Add timestamp to the curve data in the log file for functions which only support force over position / Hinzufgen des Zeitstempel zu den Kurvendaten in der Log-Datei fr Funktionen welche nur Kraft ber Position untersttzen


Release Note GSAY-A4-F0-Z4-1.4.1

Firmware: 3.8.14

Note:
- A FW update from version 3.4.6 or smaller to 3.8.14 is required and it cannot be downgraded from version 3.8.14 to 3.4.6 or smaller
- A GSDML update in the higher-level plc to the version GSDML-V2.34-Festo-CECC_X-20210401.xml is required
- An update of the host function blocks is required (New host interface)

Bugs:
* BUG-4334903 - German language settings: Numbers of digital IO's are cut in the diagnosis window / Deutsche Spracheinstellung: Nummern der digitalen IO's werden im Diagnosefenster abgeschnitten

Change Requests:
* CRQ-3086565 - Control highness - Webvisu (only) / Steuerhoheit - Webvisu (only)
* CRQ-3086667 - Software/Firmware update to SP 15 Patch 3 / Software/Firmware update auf SP 15 Patch 3
* CRQ-3086697 - Reduce Profinet IO Cylce time with new Profinet IO Stack to 10ms / Reduzierung der Profinet IO Zykluszeit mit neuem Profinet IO Stack auf 10ms
* CRQ-3086566 - Add serial number to log file name / Hinzufgen der Seriennummer zum Name der Log-Datei
* CRQ-3086681 - Add force control continue and force reached to the host-interface / Hinzufgen von Kraftregelung weiter und Kraft erreicht zur Host-Schnittstelle
* CRQ-3086568 - Add force, position and velocity limitation for manual movement / Hinzufgen einer Kraft- / Positions- / Geschwindigkeitsbegrenzung fr einen manuellen Verfahrbefehl
* CRQ-3102811 - Change adjustment force sensor values via input field / ndern der Werte der Kraftsensor Justage ber ein Eingabefeld
* CRQ-3086567 - Add the result for each criterium (window, threshold, envelope) of the recipe to the host-interface / Hinzufgen des Ergbnisses jedes einzelnen Kriteriums (Fenster, Schwellwert, Hllkurve) der Bewertungsverfahren zur Host-Schnittstelle
* CRQ-3086668 - New host-interface (Combine cyclic/acyclic mode to one mode) / Neue Host-Schnittstelle (Kombinieren von zyklischem/azyklischem Modus zu einem Modus)
* CRQ-3086688 - Record reference curve without staying in the corresponding screen / Aufnehmen der Referenzkruve ohne sich in dem entsprechenden Bildschirm zu befinden
* CRQ-3086689 - Remove german online help / Entfernen der deutschen Online-Hilfe
* CRQ-4334914 - Scrollbar for sequencer useable in operation and record reference curve window / Scrollbar fr den Sequencer benutzbar im Fenster Betrieb und Referenzkurve aufzeichnen


Release Note GSAY-A4-F0-Z4-1.3.15

Firmware: 3.8.14

Note:
- A FW update from version 3.4.6 or smaller to 3.8.14 is required and it cannot be downgraded from version 3.8.14 to 3.4.6 or smaller
- A GSDML update in the higher-level plc to the version GSDML-V2.34-Festo-CECC_X-20210401.xml is required

Bugs:
* BUGEA-5547524 - Evaluation methods -> Sporadic false OK/NOK (Window down/up side, Force threshold) / Bewertungsverfahren -> Sporadisch Falsch OK/NOK (Fenster untere/obere Siete, Kraft-Schwellwert)


Release Note GSAY-A4-F0-Z4-1.3.13

Firmware: 3.8.14

Note:
- A FW update from version 3.4.6 or smaller to 3.8.14 is required and it cannot be downgraded from version 3.8.14 to 3.4.6 or smaller
- A GSDML update in the higher-level plc to the version GSDML-V2.34-Festo-CECC_X-20210401.xml is required

Change Requests:
* CRQ-3086697 - Reduce Profinet IO Cylce time with new Profinet IO Stack to 10ms / Reduzierung der Profinet IO Zykluszeit mit neuem Profinet IO Stack auf 10ms
* CRQ-4153991 - Update FW/TSP/GSDML


Release Note GSAY-A4-F0-Z4-1.3.11

Firmware: 3.4.6

Bugs:
* BUG-2665354 - After pos. force sensor error (PM, FM, DSM) -> Error reaction will not be performerd / Nach einem pos. Kraftsensor Fehler (PM, FM, DSM) -> Fehler-Reaktion wird nicht ausgefhrt


Release Note GSAY-A4-F0-Z4-1.3.7

Firmware: 3.4.6

Bugs:
* BUG-2205075 - No error for negative time limit and holding time (via variable) in the function force control / Kein Fehler bei negativer Haltezeit und negativem Zeitlimit (ber Variable) bei der Funktion Kraftregelung
* BUG-2227009 - No data read for object "Program ID" (Changed to data type UDINT) and "Timestamp" (0x2100 - 0x16/0x17) / Keine Daten gelesen fr das Objekt "Program ID" (Wechsel zu Datentyp UDINT) und "Timestamp" (0x2100 - 0x16/0x17)
* BUG-2583349 - Start press process with Abort "False" stays in status "In operation" (PM, FM, DSM) / Pressprozess starten mit Abbruch "False" bleibt in Status "In operation" (PM, FM, DSM)
* BUG-2583355 - No movement, when perform relatvie movement after absolut movement with same value / Keine Bewegung, wenn eine relative Bewegung mit dem gleichen Wert nach einer absoluten Bewegung erfolgt

Change Requests:
* CRQ-2244513 - Automatic enable of the motor controller after homing (only necessary for Multi-Turn encoder) / Automatisches einschalten des Motorconroller nach der Referenzfahrt (nur ntig fr Multi-Turn Encoder)
* CRQ-2406432 - Change automatic internal logging to enable/disable manually / ndern der automatischen internes Logging, so dass es manuell ein- oder ausgeschaltet werden kann
* CRQ-2583366 - GUI Logging: SMB-Share,FTP-Server and Internal inactive in host control mode / GUI Logging: SMB-Share,FTP-Server und Intern in Steuerhoheit Host inaktiv

Release Note GSAY-A4-F0-Z4-1.3.5

Firmware: 3.4.6

Bugs:
* BUG-2014841 - Empty system configuration file (0kB), by switching off the system / Leere Systemkonfigurationsdati (0kB), durch Ausschalten des Systems
* BUG-2174246 - After the advanced force mode has been executed, there is a strong decrease in force/ Nachdem der advanced force mode ausgefhrt wurde, gibt es eine starke Kraftabnahme
* BUG-843862 - Intersections on windows/thresholds are not recognized because of hysteresis / Schnittpunkte an Fenstern / Schwellen werden wegen der Hysterese nicht erkannt
* BUG-2183322 - Incorrect assignment NOK cause force control / Falsche Zuordnung NOK Ursache force control
* BUG-2191488 - No reaction in position mode to abort press process (X3.5) when button is pressed very fast / Keine Reaktion im position mode auf Pressprozess abbrechen (X3.5), wenn Taster ganz schnell gedrckt wird

Change Requests:
* CRQ-2053356 - Improve the advanced force mode by using velocity mode (CMMP) instead of torque mode / Verbessern des erweiterten Kraftbetriebs indem der velocity mode (CMMP) anstatt des torque mode verwendet wird
* CRQ-2076067 - Parameter for ADV force mode/force control adjustable via variables / Parameter bei ADV force mode/force control ber Variablen einstellbar


Release Note GSAY-A4-F0-Z4-1.3.3

Firmware: 3.4.6

Bugs:
* BUG-1954666 - If you let the mouse button go too far away from the button while jogging visually, you will continue to jog / Lsst man beim Joggen per Visu die Maustaste zu weit entfernt vom Button los, so wird immer weiter gejoggt
* BUG-1967814 - Max. position/force in the tab operation are different to the tab diagnosis (Advanced force mode/Force control) / Max. Position/Kraft im Tab Betrieb sind unterschiedlich zum Tab Diagnose (Erweiterter Kraftbetrieb/Kraftregelung)
* BUG-1971489 - Selection menu remains in the visu with the function "Jump" in the sequencer / Auswahlmenu bleibt  in der Visu erhalten bei der Funktion "Jump" im Sequenzer
* BUG-1999635 - Random EtherNet/IP communication interrupts / Zufllige EtherNet / IP-Kommunikationsunterbrechungen
* BUG-1999638 - Translation errors in different languages / bersetzungsfehler in den verschiedenen Sprachen
* BUG-2004125 - Incorrect axis label text is displayed in the function "Adjustment force sensor" / Falscher Achsbezeichnungstext wird in der Funktion "Justage Kraftsensor" angezeigt
* BUG-2005781 - Not possible to insert float values in the function "Error reaction" in the sequencer / Es ist nicht mglich Gleitkommazahlen in der Funktion "Fehlerreaktion" im Sequenzer einzugeben
* BUG-2012956 - Evaluation methods windowing and threshold do not work on very steep curves / Bewertungsverfahren Fenstertechnik und Schwellwerte funktionieren bei sehr steilen Kurven nicht
* BUG-874823 - Variables are not written sporadically via host / Variablen werden ber Host sporadisch nicht geschrieben
* BUG-1971488 - In the function advanced force mode the press moves randomly until a force sensor error / In der Funktion erweiterter Kraftbetrieb frht die Presse sporadisch bis zu einem Kraftsensor Fehler
* BUG-1991683 - Exception error on save program - Time limit is greater than 38s for a record (Advanced force mode/Kraftregekung) / Ausnahmefehler beim Programm speichern - Zeitlimit grer als 38s fr eine Aufzeichnug ist (Erweiterter Kraftbetrieb/Kraftregelung)

Change Requests:
* CRQ-1996470 - Dynamic adjustment of the recording interval in the force-time diagram depending on the holding time / Dynamische Anpassung des Aufzeichungsintervalls im Kraft-Zeit Diagramm abhngig von der Haltezeit


Release Note GSAY-A4-F0-Z4-1.3.1

Firmware: 3.4.6

Note: 
- Function of digital input X17.4.2 changed from safety feedback to servo press activation

  Webvisu and Digital IO mode: Manual enable/disable of the motor controller via digital input X17.4.2 (rising edge = enable / fallinge edge = disable).
			       No autmoatic enable/disable of the motor controller anymore.	
					
  Host mode: Manual enable/disable of the motor controller via control word bit 7 (Host-FB input "xEnableSystem") (rising edge = enable / fallinge edge = disable).
	     No autmoatic enable/disable of the motor controller anymore.	

Bugs:
* BUG-875464 - Empty system configuration file blocks the initialization / Leere Systemkonfigurationsdatei blockiert die Initialisierung
* BUG-881964 - Message window remains in the foreground / Nachrichten Fenster bleibt im Vordergrund erhalten
* BUG-882564 - Empty logging internal file error is not possible to quit / Leere Logging intern Datei Fehler kann nicht quittiert werden
* BUG-958083 - FTP-Server error - Simultaneous write to FTP-Server by more YJKP / FTP-Server Fehler - Gleichzeitiges Schreiben auf FTP-Server durch mehr YJKP
* BUG-961230 - FTP-Server URL not reset via Cancel to old value / FTP-Server URL wird bei Abbrechen nicht auf den alten Wert zurckgesetzt
* BUG-1973007 - Execute logging FTP and internal even in case of error logging to SD card or USB stick / Ausfhren von Logging FTP und Internal auch im Fehlerfall beim Logging auf SD-Karte oder USB-Stick

Change Requests:
* CRQ-307746 - Show step time of a step in the sequencer / Anzeigen der Schrittzeit eines Schrittes im Sequenzer
* CRQ-429209 - Transfer a serial number via host and add it to the log file / bertragen einer Seriennummer ber Host und hinzufgen dieser in der Log-Datei
* CRQ-429252 - Installation of a force control / Einbau einer Kraftregelung
* CRQ-430637 - NOK reason as clear text within visualization / NIO Grund in der Visualisierung als Klartext anzeigen
* CRQ-435921 - Add MAC Address to the log file and make it available via host / Hinzufgen der MAC-Adresse in der Log-Datei und ber den Host verfgbar machen
* CRQ-454046 - Highlight the input fields in the side window more clearly / Eingabefelder im seitlichen Fenster deutlicher hervorheben
* CRQ-456238 - Simplify the selection of the hardware configuration / Vereinfachen der Auswahl der Hardware-Konfiguration
* CRQ-481892 - Change program ID to lifetime counter / ndern der Programm ID zu einem Lebensdauerzhler
* CRQ-489958 - Save the settings for show diagram / Speichern der Einstellungen fr die Anzeige des Diagramm
* CRQ-506531 - Name sequencer steps / Bennen der Schritte im Sequenzer
* CRQ-506671 - Set system time manually / Systemzeit manuell setzen
* CRQ-510424 - Program step mode via IO / Programmschrittbertrieb ber E/A
* CRQ-525274 - Sequencer error reaction / Sequenzer Fehlerreaktion
* CRQ-531699 - Add OK/NOK result and cycle time calculation to record reference curve / Hinzufgen des Resultat IO/NIO und Zykluszeitberechung zur Aufnahme der Referenzkurve
* CRQ-495333 - Manual enable/disable of the motor controller (Reduce cycle time) / Manuelles einschalten/ausschalten des Motorconroller (Zykluszeit verringern)
* CRQ-558090 - Show reference curve in the operation window possible / Anzeigen der Referenzkurve im Betriebsfenster mglich
* CRQ-429836 - Increase axis labeling in all diagrams / Vergrern der Achsbezeichnungen in allen Diagrammen
* CRQ-924214 - Installation of a advanced force mode / Einbau eines erweiterten Kraftbetrieb
* CRQ-941611 - Change the prioritization of the NOK reason for several NOK reasons / ndern der Prioriserung des NIO Grundes bei mehreren NIO Grnden
* CRQ-958576 - New logging functionality SMB-Share / Neue Logging-Funktionalitt SMB-Share
* CRQ-510423 - Show the max. last 5 curves or custom curves as series of curves / Anzeigen der max. letzten 5 Kurven oder kundenspezifischer Kurven als Kurvenschar
* CRQ-515878 - OPC-UA connection / OPC-UA Anbindung
* CRQ-630855 - Jump function with comparison / Sprung-Funktion mit Vergleich
* CRQ-1972992 - Login button only active after initialization / Einloggen Button erst aktiv nach der Initialisierung
* CRQ-1973023 - Licensing of functionalities / Lizenzierung von Funktionalitten


Release Note GSAY-A4-F0-Z4-1.2.1

Firmware: 3.4.6

Bugs:
* BUG-619410 - Homing signal will be lost shortly after homing (Singleturn motor mounted / Multiturn motor selected) / Referenzfahrt-Signal wird kurze Zeit nach der Referenzfahrt verloren (Singleturn-Motor verbaut / Multiturn-Motor ausgewhlt)
* BUG-693856 - Enable of the motor controller without hardware inputs occurs error (Right status is not possible to enable anymore)  / Enabeln des Motorcontroller ohne Hardware-Eingnge verursacht einen Fehler (Im richtigen Zustand ist es nicht mehr mglich zuenablen)
* BUG-693869 - Missing error reaction to some errors and all warnings / Fehlende Fehlerreaktion auf manche Fehler und alle Warnungen
* BUG-694157 - Quit error during active warning (Afterwards it is not possible to quit a error) / Fehler quittieren whren einer aktiven Warnung (Danach ist es nicht mehr mglich einen Fehler zu quittieren)
* BUG-588492 - The loaded program number over the host interface at start up is always zero / Die geladene Programmnummer ist ber das Host-Interface bei Neustart Null
* BUG-600910 - Typing error in text field in the commissioning screen / Schreibfehler in einem Textfeld im Inbetriebnahme-Bildschirm
* BUG-642383 - PID settings are not correct in some hardware configuration / PID-Einstellungen sind in manchen Hardware Kontigurationen nicht korrekt
* BUG-694147 - Read wrong recipe envelope data (Recipe 2-5 Envelope 2-5) via host / Auslesen der falschen Hllkurven-Daten (Bewertungsverfahren 2-5 Hllkurve 2-5) ber Host
* BUG-694150 - Wrong NOK source is displayed when NOK source is unequal position mode / Falsche NIO-Ursache wird angezeigt, wenn die NIO-Ursache ungleich Positioniermodus ist
* BUG-694151 - Quit errors independent from each other, when more then one is present (i.e. CAN-Bus error +  Safety error) / Fehler unabhngig voneinader quittieren, wenn mehr als ein Fehler anliegt (z.B. CAN-Bus Fehler + Safety Fehler)
* BUG-694152 - Jog command has to be done two times to get movement in the host plc / Jog-Befehl muss zweimal in der Host-Steuerung ausgefhrt werden fr eine Bewegung
* BUG-756264 - A wrong info 2 is shown in case of error Save on USB (0xFF000134/0x00000008) / Eine falsche Info 2 wird im Fall des Fehler Speichern auf USB (0xFF000134/0x00000008) angezeigt
* BUG-665886 - Empty program numbers can occur when selecting program slot in the list via Host / Es knnen leere Programmspeicherpltze bei der Auswahl ber Host entstehen
* BUG-746301 - Error reaction after quit a error enable motor controller is not correct / Fehler-Reaktion nach quittieren eines Fehlers Enablen des Motorcontrollers ist nicht richtig

Change Requests:
* CRQ-363025 - Program selection via IO / Programmumschaltung ber EA
* CRQ-431160 - Add more languages to WebVisu / Hinzufgen weiterer Fremdsprachen zu WebVisu
* CRQ-307730 - Save complete logging curves (Force over stroke) / Speichermglichkeit Logging Kurven speichern (Kraft ber Weg)
* CRQ-429206 - Error codes as clear text within visualization / Fehlercodes in der Visualisierung als Klartext anzeigen
* CRQ-429211 - Adjustment force sensor / Justage des Kraftsensor
* CRQ-438134 - Add variable number in variable step within sequencer overview / Anzeige der Variablennummer in der Sequenzerbersicht
* CRQ-450153 - Visual feedback if press is in manual and auto mode / Feedback ob sich die Presse in Manual oder Automodus befindet.
* CRQ-460947 - More meaningful designation of the status of the press in the visualization / Ausgefhigere Bezeichnung vom Status der Presse in der Visualisierung
* CRQ-488566 - Hide passwort input / Versteckte Passworteingabe
* CRQ-513425 - Add button to save the program in any window of edit program / Button zum Speichern der Programmerstellung in jedem Fenster zur Verfgung stellen
* CRQ-548952 - Changing Auto to Manual has no effekt on a ongoing process / Wechsel von Auto zu Manual hat keine Auswirkung auf einen laufenden Prozess
* CRQ-559787 - New screen for interface diagnosis (Live View for DIO, Analogue Input and Bus data) / Neuer Bildschirm fr Schnittstellendiagnose (DIO, Analogwerte und Busdaten)
* CRQ-560273 - Deactivate button "Load" if contorl highness is "Host" / Button "Laden" deaktivieren bei der Steuerhoheit "Host"
* CRQ-594819 - Software support of 2 hand control and STO/SS1 / Software Untersttzung der Zweihandbedienung und STO/SS1
* CRQ-429233 - Support Profinet IO/ Untersttzung Profinet IO
* CRQ-693858 - Start FTP-Server automatically at initialization / Automatisches Starten des FTP-Server bei der Initialisierung
* CRQ-693861 - Get status of homing via the statusword of the motorcontroller / Referenzfahrterkennung ber das Statuswort des Motorcontroller
* CRQ-694158 - Relieve when the positive/negative force limit is reached / Freifahren bei Erreichen des positiven/negativen Grenzwertes des Kraftsensors
* CRQ-653754 - Reorganize of the logging of the press data + New logging functionallity FTP-Server / Umgestalten des Loggen der Pressdaten + Neue Log-Funktionalitt FTP-Server
* CRQ-694144 - Reduce value for cable break detection / Wert fr die Kabelbrucherkennung heruntersetzen
* CRQ-766751 - Program name only allow the following signs (a-z, A-Z, 0-9 and _) / Programmname erlaubt nur die folgenden Zeichen (a-z, A-Z, 0-9 and _)


Release Note GSAY-A4-F0-Z4-1.1.1

Firmware: 3.2.10

Bugs:
* BUG-438127 - No adjustment of the diagram size if the evaluation methods are outside the diagram / Keine Anpassung der Diagrammgre, wenn die Bewertungsverfahren auerhalb des Diagramms liegen
* BUG-453143 - Read objects from object 0x3000 via the host interface / Auslesen der Objekte ab Objekt 0x3000 ber das Host-Interface
* BUG-453147 - Calculation of the intersection of the envelope curve / Berechnung der Schnittpunkte der Hllkurve
* BUG-453150 - Error in digital signal mode in the evaluation of the relative path / Fehler bei der Auswertung des relativen Weges im digitalen Signalmodus
* BUG-453213 - The live view of the sequence while recording a reference curve doesn't scroll down automatically / Die Live-Anzeige der Sequenz bei der Aufnahme einer Referenzkurve srollt nicht automatisch runter
* BUG-453216 - Hysteresis for the force is currently missing for the evaluation methods / Hysterese fr die Kraft bei den Bewertungsverfahren fehlt
* BUG-460872 - Press process no longer starts after the CAN bus communication has been terminated (only when using singelturn motors) / Pressprozess startet nach Verbindungsabbruch der CAN-Bus Kommunikation nicht mehr (nur bei Verwendung von Singelturn Motoren)
* BUG-476860 - The result of reading "Max. position" and "Max. force" over the host interface is always zero / Auslesen der "Max. Position" und "Max. Kraft" ber das Host-Interface ergibt immer Null
* BUG-480166 - Read OK/NOK result over host-interface keep status when a new press process has been started / Beim Auslesen des IO/NIO Ergebnis ber das Host-Interface wird der Status behalten wenn ein neuer Pressprozess gestartet wurde
* BUG-481729 - The virtual digital outputs (Bit 0-7) are not transferred over the host interface / Die virtuellen digitalen Ausgnge (Bit 0-7) werden nicht ber das Host-Interface bertragen
* BUG-481730 - The digital outputs are not reset when starting a press process / Die digitalen Ausgnge werden beim Starten eines Pressprozesses nicht zurckgesetzt
* BUG-481792 - If the analog input is exceeded, an incorrect force value is displayed / Bei Bereichsberschreitung des analogen Eingangs wird ein falscher Kraftwert angezeigt
* BUG-481859 - In the process diagnosis the program name is not shown / In der Prozessdiagnose wird der Programmname nicht angezeigt
* BUG-481894 - In the process diagnosis the wrong ID is shown in the table / In der Prozessdiagnose wird die falsche ID in der Tabelle angezeigt
* BUG-490182 - Settings of logging in WebVisu and Host are different / Einstellungen fr das Logging sind in der WebVisuund Host unterschiedlich
* BUG-516328 - Design of current limitation / Auslegung der Strombegrenzung
* BUG-516329 - Evaluation of max. force with constant negative force values / Auswertung der max. Kraft bei konstant negativen Kraftwerten
* BUG-531522 - Auto scaling of recorded return stroke doesn't work correctly / Automatische Skalierung eines aufgenommenen Rckhubs funktioniert nicht richtig
* BUG-531527 - Auto-scaling of loaded referenced curve doesn't work / Automatische Skalierung funktioniert nicht bei einer geladenen Referenzkurve
* BUG-531541 - "Read analog force value" error can't be acknowledged / "Einlesen des analogen Kraftwertes" Fehler kann nicht quittiert werden
* BUG-531579 - Save program / Programm speichern
* BUG-532590 - Homing can not be aborted / Referenzfahrt kann nicht abgebrochen werden
* BUG-539910 - Error in digital signal mode and force mode in the evaluation of a negative relative path / Fehler bei der Auswertung des negativen relativen Weges im digitalen Signalmodus und Kraftmodus
* BUG-544331 - Wrong window is displayed by click on button "Back" in the window "Configure monitoring - Windowing" / Falsches Fenster wird angezeigt beim Klicken auf den Button "Zurck" im Fenster "berwachung konfigurieren - Fenstertechnik"
* BUG-544793 - The returned program number in the higher-level control is only a reflection of the selected program number / Die zurckgelieferte Programmnummer in der bergeordneten Steuerung ist nur eine Spiegelung der ausgewhlten Programmnummer
* BUG-546400 - Homing is not possible in case of an error or warning / Referenzfahrt im Fehler- /Warnungsfall nicht mglich
* BUG-546402 - Undefined state in case of an emergency stop / Undefinierter Zustand auf Grund eines Not-Aus
* BUG-546411 - Not all messages are selectable if there are multiple messages / Es sind nicht alle Nachrichten auswhlbar, wenn es mehrere Nachrichten gibt

Change Requests:
* CRQ-480165 - Delete timeout for read input (60s) / Timeout fr Eingang lesen (60s) entfernen


Release Note GSAY-A4-F0-Z4-1.1.0

Firmware: 3.2.10

- Initial version